Jump to content
OMRON Forums

Help understanding ACC-28E inputs


dennisg

Recommended Posts

I am adding an input (CH3) to our 4 channel ACC-28E A-D board. The only manual I can find references the UMAC-TURBO.

 

Where can I find the info I need to set this input up on Motor[6] so I can read it from a PLC ?

 

TIA.

Link to comment
Share on other sites

  • Replies 4
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

dennisg,

 

Please check the , under section titled: "Acc28E Status Data Structure Elements".http://forums.deltatau.com/filedepot/download.php?f=Power%20PMAC/Manuals/Power%20PMAC%20Software%20Reference%20Manual.pdf [FILE REMOVED]

 

In order to read an analog input, you don't have to assign it to a motor. You can either read the Acc28E.AdcSdata[j] or Acc28E.AdcUdata[j] directly, or you can define your own custom name for it:

#define InputTemp Acc28E[0].AdcSdata[0]

 

If you want to read the analog feedback as an input to a motor servo loop, you should read the input using encoder conversion table, which is explained in the , under the section titled: "Setting Up the Encoder Conversion Table". You should use entry Type 1: Single-Register Parallel Read.http://forums.deltatau.com/filedepot/download.php?f=Power%20PMAC/Manuals/Power%20PMAC%20User [FILE REMOVED]

Link to comment
Share on other sites

dennisg,

 

Please check the , under section titled: "Acc28E Status Data Structure Elements".http://forums.deltatau.com/filedepot/download.php?f=Power%20PMAC/Manuals/Power%20PMAC%20Software%20Reference%20Manual.pdf [FILE REMOVED]

 

In order to read an analog input, you don't have to assign it to a motor. You can either read the Acc28E.AdcSdata[j] or Acc28E.AdcUdata[j] directly, or you can define your own custom name for it:

#define InputTemp Acc28E[0].AdcSdata[0]

 

If you want to read the analog feedback as an input to a motor servo loop, you should read the input using encoder conversion table, which is explained in the , under the section titled: "Setting Up the Encoder Conversion Table". You should use entry Type 1: Single-Register Parallel Read.http://forums.deltatau.com/filedepot/download.php?f=Power%20PMAC/Manuals/Power%20PMAC%20User [FILE REMOVED]

 

Thanks Sina, is there anything I have to do to specifically enable 3 & 4? I ask because I see the expected raw data on 1 & 2 (Acc28E[1].AdcUdata[0].a, Acc28E[1].AdcUdata[1].a) but not 3 (Acc28E[1].AdcUdata[2].a).

Link to comment
Share on other sites

Are you sure you have a 4 channel version of ACC-28E and not a 2 channel one?

 

Thanks to CharlesP there who was kind enough to send me a new unreleased draft version of the ACC-28 manual which I found easier to read, I was able to determine we did indeed only have a 2 channel board. I did some looking around here and found another 2 channel and brought it up for my 3rd channel.

Link to comment
Share on other sites

Guest
This topic is now closed to further replies.

×
×
  • Create New...