biocat Posted November 19, 2012 Posted November 19, 2012 I'm using Power PMAC IDE to do Test and Commission the motor. My hardware are ACC-24E2A and AMP-1 4-axis linear amplifier. This servo motor has been tested in other channels without problem. But in one channel, I got the Debug Message as below. Even I changed the direction, it still didn't work. Could somebody help me? Thanks! 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Arguments Entered: 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Motor Number: 2 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Maximum open loop command percentage: 100.000000 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop command duration (msec): 800.000000 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Number of iterations: 2 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 20.000000% command output 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities : 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 40.000000% command output 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities : 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 60.000000% command output 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities : 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 80.000000% command output 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities : 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 100.000000% command output 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities : 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 120.000000% command output 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities : 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Feedback direction didn't match the commanded output direction! 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Continuing with the setup with current settings can be dangerous. 11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Please change the direction of feedback and start the test over again. 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - FeedbackSetup : Graph Control Connected 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Graph Control Connected 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Arguments Entered: 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Motor Number: 2 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Maximum open loop command percentage: 100.000000 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop command duration (msec): 800.000000 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Number of iterations: 2 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 20.000000% command output 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities : 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 40.000000% command output 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities : 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 60.000000% command output 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities : 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 80.000000% command output 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities : 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 100.000000% command output 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities : 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 120.000000% command output 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities : 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Feedback direction didn't match the commanded output direction! 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Continuing with the setup with current settings can be dangerous. 11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Please change the direction of feedback and start the test over again.
curtwilson Posted November 20, 2012 Posted November 20, 2012 Did you get motor motion in these tests? If you did get motion, did PMAC detect it? If you turn the motor by hand, do you see the motor position in the IDE's position window change? Most likely, something in the encoder hardware or the software that processes it is not working properly, so PMAC thinks the motor is not moving.
Recommended Posts