Jump to content
OMRON Forums

Decimal places


PEERPSI

Recommended Posts

I'm having troulbe sorting out why my program position and DTG windows are not showing the right number of decimal places. I've set them for 3.6 in inch, 3.5 in mm. They only show 4 decimal places. When I call up the "all" position window they show 6 in inch, sometimes. It seems to change if you try a reboot.

 

Also my Program position window is not titled Program position buy absolute?

 

Stranger yet is the fact that it was all working right. I had an incorrect value for maximum feedrate so I reran auto pilot making the change I needed. Since doing that it has not worked right.

 

Any ideas?

Link to comment
Share on other sites

  • Replies 1
  • Created
  • Last Reply

Top Posters In This Topic

Top Posters In This Topic

Guest
This topic is now closed to further replies.

×
×
  • Create New...