FWTech Posted May 15, 2013 Share Posted May 15, 2013 I put a Copley ESI xml file under the ECATDeviceFiles folder and take the following steps to set up offline a slave device. 1. Right click on the Master[0] Deactivated and click on "Append Device". 2. Select a drive and then click "Add Device". However, the Setup Messages show "Default device file is not defined for ..." and no any device appears under the Amplifiers. The attached screen shot shows this case. Link to comment Share on other sites More sharing options...
Recommended Posts