naguiman Posted May 22, 2013 Share Posted May 22, 2013 Hello.. My customer has resolver feedback. Resolver Spec -------------- Rotor 1phase (INPUT) 26Volts Stator 2Phase (OUTPUT) 11.8Volts Frequency 400Hz Does ACC-58E accept this resolver type? Link to comment Share on other sites More sharing options...
curtwilson Posted May 23, 2013 Share Posted May 23, 2013 No, the resolver at these levels is not compatible with the ACC-58E. The excitation output from the ACC-58E is a maximum of 7Volts (peak-to-peak), and the feedback values should be 1-2Volts p/p. Also, it was designed to use resolver frequencies over 1000 Hz. Link to comment Share on other sites More sharing options...
Recommended Posts