Greg_Murphy Posted June 13, 2013 Share Posted June 13, 2013 Hi I have an Older Turbo UMAC CPU that won't store its IP address. If the instruction in the thread (link below) are followed, then the IP address can be changed, but it is lost on power up: http://forums.deltatau.com/showthread.php?tid=730 This particular hardware revision does not have a Jumper E1 (Board # 603766-104). The closest thing I've found is a set of solder pads labelled CE1 near the USB/Ethernet chip. Access via the ethernet port is more of a convenience, so this problem is really a question of why, and can it be easily fixed? Please let me know if you have any questions, or if you would like any additional information. Cheers Greg Link to comment Share on other sites More sharing options...
Omron Forums Support Posted June 13, 2013 Share Posted June 13, 2013 Hi Greg, That sounds like a hardware failure. You could try reloading com firmware. Here is a forum link to instructions: http://forums.deltatau.com/showthread.php?tid=63&highlight=firmware. Link to comment Share on other sites More sharing options...
Greg_Murphy Posted June 14, 2013 Author Share Posted June 14, 2013 Hi Gregs, Thank you for the link. The firmware download as per the Forum link worked a treat - the UMAC is now remembering its IP Address! Using Windows 7, I needed to use the "Devices and Printers" (located under "Hardware and Sound" in the Control Panel, or direct from the Start Menu depending on setup) instead of the Device Manager mentioned at Step 2 of the Forum link you provided. Once again, thank you. Cheers Greg Link to comment Share on other sites More sharing options...
Omron Forums Support Posted June 17, 2013 Share Posted June 17, 2013 Hello Greg, Glad to hear it is working. I am surprised that USB did not display in Device Manager but did elsewhere. It should be seen in Device Manager now, now that there is communication. Link to comment Share on other sites More sharing options...
Recommended Posts