dorcsssc Posted July 16, 2013 Share Posted July 16, 2013 Did I miss something near the end of the User's Guide about this? Or did I misunderstand an IDE menu item along these lines? Now that we're basically satisfied with the functioning of our background C application, we want to burn it into our PPMAC so that it will run whenever powered up, without the IDE. Please tell us how our production operators can run a PPMAC with this application without obliging them also to use the IDE. Thanks. Link to comment Share on other sites More sharing options...
Sina.Sattari Posted July 16, 2013 Share Posted July 16, 2013 You can set each Background C App to start up automatically upon Power Up/Reset/Project Load process using the following steps: 1. In solution explorer window, right click on the desired C-App folder and select properties. 2. Under CPLC Startup option, select Yes for Run at startup setting. 3. Build and download the project to Power PMAC. 4. Issue a SAVE command in the terminal window. Link to comment Share on other sites More sharing options...
Recommended Posts