Jump to content
OMRON Forums

Recommended Posts

Posted

I'm using a ACC - 24E2S card in the 4th slot. It is the 4th Servo IC.

 

The thing is that the 4th Servo IC is configured the same way the 3rd Servo IC is. They are both 24E2S and both are used for the same thing, controlling a driver that makes the commutation. However, the 4th Servo IC enables the driver without sending any pulse or direction to the driver, and so, the motor does not move. The 3rd Servo IC works just fine.

 

For the second channel of the 4th Servo IC Im using the attached configuration, and the motor 6 is configure as the attached file shows.

 

I have no idea what can be wrong, since the 3rd card works with the same setup (changing some addresses). Please Help.

Setup_motor_6.txt

Setup_Servo_IC_4.txt

  • Replies 0
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

Guest
This topic is now closed to further replies.

×
×
  • Create New...