paddax Posted July 24, 2013 Share Posted July 24, 2013 We are using a Turbo UMAC and Macro to connect to a set of Copley drives. When performing a move until trigger the system works most of the time, however occasionally the trigger is missed and the axis continues until the target position. Move until trigger command is as follows X(M140)^0Y(M141)^0Z(M142)^0 I can't get any further with this problem as the entire process is controlled in the protocol between the UMAC and the Copley drives. Link to comment Share on other sites More sharing options...
Recommended Posts