bigprinters Posted August 14, 2013 Share Posted August 14, 2013 Do you have a problem in xp all of a sudden where you can test an ip address but cannot connect to the device. I am wondering if a firewall setting has caused a problem in PCommServer. Any thoughts? Link to comment Share on other sites More sharing options...
Unit101 Posted August 21, 2013 Share Posted August 21, 2013 I have seen this where you had a duplicate IP on network... so the PING test succeeds... but it is being fooled since it is not really a PMAC making the reply. So the Test is OK... but can't connect since not really reaching the PMAC device. So are you directly connected to PMAC or thru a larger network ? I've never seen a typical firewall setup cause issue... disable the firewall and test ? Link to comment Share on other sites More sharing options...
Recommended Posts