daves Posted September 13, 2013 Share Posted September 13, 2013 As I have changed the IP address of particular cards I download to I have ended up with a large amount of files called 192.168.0.200_INIFile.ini 192.168.0.200_pp_debug.txt 192.168.0.200_ppError.Log 192.168.0.200_ppErrorHist.Log 192.168.0.200_ppProj.Log 192.168.0.200_temppp_proj.h PPMAC_192.168.0.200_INIFile.ini 192.168.0.202_INIFile.ini .... etc for each IP address ever used, all bunged in the project folder. Is it necessary to store whatever these files are like this? I assume I can just delete all but the currently in use ones? What is in them, is it generated on download or is it something which needs to go in my version control system? Cheers Dave Link to comment Share on other sites More sharing options...
Recommended Posts