LECA1239 Posted January 16, 2014 Share Posted January 16, 2014 Hi, we are using presently Geobrick with Turbo Pmac, we now want use Brick controller with Power Pmac, will Pmac work with following drives which has SSCNET III/H The motor we have selected will work with only MRJ4 drives. MRJ4 drives will work with SSCNET III/H which is high speed communication (150 mbps) as compare to SSCNET III(50 mbps). However MRJ3 drives support only up to 15 mbps speed. With SSCNET III/H, we can update position command in the drive in 0.22 ms. Also MRJ4 drive is with versatile features for tuning and adaptive vibration suppression features. With 22 bit encoder, we can use only MRJ4 drive. Please share any information is any one using with SSCNET III/Hsscnet.pdf Link to comment Share on other sites More sharing options...
Omron Forums Support Posted January 16, 2014 Share Posted January 16, 2014 From looking at the document you attached, I cannot really determine what sort of control signal the amplifier receives, nor can I determine whether the drive returns simulated quadrature to PMAC. Do you know these things? Or, can you attach pinouts for wiring the amplifier? Link to comment Share on other sites More sharing options...
curtwilson Posted January 16, 2014 Share Posted January 16, 2014 SSCNET is a network interface that requires a custom interface with a special ASIC. We are evaluating the requirements for building this interface now, but designing the necessary hardware and software for a interface like this is a major development task. Link to comment Share on other sites More sharing options...
tecnico Posted January 14, 2016 Share Posted January 14, 2016 Using a lot of Mitsubishi stuff for me SSCNET support would be really nice. Not sure if after Omron's takeover is there any interest in adding compatibility with a competitor. Link to comment Share on other sites More sharing options...
Recommended Posts