daves Posted January 29, 2014 Share Posted January 29, 2014 I have the following in my standard PPMAC code (which originally came from Turbo code): // Bits 0-23 are inputs, bits 24-47 are outputs // Set up Acc65E card GateIo[0].CtrlReg = $07; Phase II of my code has the acc65e being transferred over MACRO. Do I need to set this for my card and if so how do I do it through the MACRO CPU? It appears to be working without setting this but the help says "This setting is strongly recommended" Link to comment Share on other sites More sharing options...
daves Posted February 18, 2014 Author Share Posted February 18, 2014 As an answer for myself I found a reference to the control word over MACRO in the Acc14E manual, so I'm going to use that: cmd "MacroSlave0, I198 = $408807"; cmd "MacroSlave0, I199 = $7"; I hope it is right Link to comment Share on other sites More sharing options...
Recommended Posts