Jump to content
OMRON Forums

Windows 7 64 bit driver for old ACC54E needed


faitjx

Recommended Posts

I have a couple of old Acc54E turboPMAC2 systems that I need the USB driver for that will work with windows 7 64bit. When I plug in the USB, the system cannot find a driver for the device. It shows up in Device Manager as a EZ-USB device, with no driver. I have installed the latest version of the PEWIN32, and have configured the system so that the programs run as administrator, giving them the access they might possibly need.

As Windows never loads a driver, it never gets to the point of being able to add the PMAC to the communications library.

 

Any suggestions are welcome. I cannot power cycle the PMAC, however, as it is actively in use via serial communications, and I don't want to have to home 24 motors.

Link to comment
Share on other sites

  • Replies 1
  • Created
  • Last Reply

Top Posters In This Topic

Top Posters In This Topic

Guest
This topic is now closed to further replies.

×
×
  • Create New...