prbt Posted October 21, 2014 Share Posted October 21, 2014 Hi, I purchased an ACC-68E with Sinking Ultra(Pn: 3-3595A-00-0000-B200). 1) For the card, 24 IN/24 OUTPUT are all configured as sinking. However, ACC-68E user manual(Ver. 2014 Feb) writes that the inputs can only be configured as sourcing on Page 8. I am puzzled at that. 2) According to following digital wiring diagram for S700 drive by Kollmorgen, an output from 68E needs to be connected to DIGITAL-IN1 to reset drive fault. I wonder if the sinking configuraion works. Or I have to purchase one more 68E with sourcing outputs. 3) An ACC-24E3(Pn: 3-4002A6666-3232-B00) is also purchased. For amplifier-enable output signal, can AE_NO_x of 24E3 be connected to Enable of S700 and AE_Com_x to DGND and XGND of S700? It seems that S700 is a sourcing drive. I wonder if the amplifier-enable of 24E3 can be configured for a sourcing or a sinking output. If it can, how to do it? Thank you! Link to comment Share on other sites More sharing options...
prbt Posted October 21, 2014 Author Share Posted October 21, 2014 Hi, I purchased an ACC-68E with Sinking Ultra(Pn: 3-3595A-00-0000-B200). 1) For the card, 24 IN/24 OUTPUT are all configured as sinking. However, ACC-68E user manual(Ver. 2014 Feb) writes that the inputs can only be configured as sourcing on Page 8. I am puzzled at that. 2) According to following digital wiring diagram for S700 drive by Kollmorgen, an output from 68E needs to be connected to DIGITAL-IN1 to reset drive fault. I wonder if the sinking configuraion works. Or I have to purchase one more 68E with sourcing outputs. 3) An ACC-24E3(Pn: 3-4002A6666-3232-B00) is also purchased. For amplifier-enable output signal, can AE_NO_x of 24E3 be connected to Enable of S700 and AE_Com_x to DGND and XGND of S700? It seems that S700 is a sourcing drive. I wonder if the amplifier-enable of 24E3 can be configured for a sourcing or a sinking output. If it can, how to do it? Thank you! Link to comment Share on other sites More sharing options...
steve.milici Posted October 21, 2014 Share Posted October 21, 2014 1. The inputs on this card are activated with a conducting ground connection if the respective return connection is 12-24 VDC. The input ground connection must be referenced to this power supply. 2. The ouputs will conduct to ground referenced to the 12-24 VDC power supply used on the ouputs connector. This must also be referenced by the drive. 3. The drive appears to use a conducting ground connection for the enable. So the AE_NO_x of 24E3 should be connected to the enable of of the drive referenced toground through AE_Com_x (ground of the drive). If you continue to have issues please contact our technical support group at support@deltatau.com or 1-818-717-5656. Link to comment Share on other sites More sharing options...
steve.milici Posted October 21, 2014 Share Posted October 21, 2014 1. The inputs on this card are activated with a conducting ground connection if the respective return connection is 12-24 VDC. The input ground connection must be referenced to this power supply. 2. The ouputs will conduct to ground referenced to the 12-24 VDC power supply used on the ouputs connector. This must also be referenced by the drive. 3. The drive appears to use a conducting ground connection for the enable. So the AE_NO_x of 24E3 should be connected to the enable of of the drive referenced toground through AE_Com_x (ground of the drive). If you continue to have issues please contact our technical support group at support@deltatau.com or 1-818-717-5656. Link to comment Share on other sites More sharing options...
Recommended Posts