KEJR Posted January 26, 2015 Share Posted January 26, 2015 Hello, I recently upgraded to the latest IDE and firmware (IDE 2.0 with Firmware 1.6.1.1). My application was hanging and seg-faulting and I was not getting any Send() messages (These may not be related). I like to use the unsolicited messages as a debugging tool when things go south. I created a simple C application in the IDE which initialized the library and sent some messages through printf() and Send(). I was not able to get the Send() function to work properly. I did verify that the unsolicited messages window in the application was started and online (several times!). I've attached the test code I'm using: #include // Global Gp Shared memory pointer //------------------------------------------------------------- // The following is a projpp created file from the User defines //------------------------------------------------------------- #include "../../Include/pp_proj.h" //Main entry point to program that also sets up threads and inits libraries. int main(void) { printf("\nAt Very Beginning\n"); /* Avoids memory swapping for this program */ mlockall(MCL_CURRENT|MCL_FUTURE); InitLibrary(); //Init DT library. printf("PPMAC is initialized.\n"); Send(1,"This is a test."); CloseLibrary(); } Please let me know if there are any ideas to try. Thanks, KEJR Link to comment Share on other sites More sharing options...
KEJR Posted January 26, 2015 Author Share Posted January 26, 2015 Sometimes its the simple things that get you. The new IDE installation didn't have the send buffers enabled that I was using (Buffers #1 and #2). I don't recall if prior versions had 0-4 as a default or if that's what I had set up originally. I was about to run sendgetsends over SSH when it occurred to me that all buffers weren't enabled. Thanks, KEJR Link to comment Share on other sites More sharing options...
Recommended Posts