odoardo Posted May 26, 2015 Share Posted May 26, 2015 HI, With Power Brick AC I want use different external analog signals as servofeedback in order to implement position following in different mode. If I acquire two analog signals in : ADC1 of connector X9. ADC1 of connector X10. is right do this? PTR ADC1X9 ->S.IO:$900028.16.16; PTR ADC1X10->S.IO:$900128.16.16; 1- Configuring two ECT entry for the two different analog signal ----------------------------------- EncTable[41].pEnc = ADC1X9; . . . . ------------------------------------ ------------------------------------ EncTable[42].pEnc = ADC1X10; . . . . ------------------------------------ 2- To change analog servo feedback change only this command (using "pmatch") Motor[9].pMasterEnc = EncTable[41].a pmatch Motor[9].pMasterEnc = EncTable[42].a In power brick Ac user manual at page 58 is written: EncTable[41].pEnc = PowerBrick[0].Chan[0].AdcAmp[2].a; But the device in this way how can distinguish between ADC1X9 and ADC1X10?? Thanks for the reply. Link to comment Share on other sites More sharing options...
steve.milici Posted May 26, 2015 Share Posted May 26, 2015 They are enumerated in this order: X9 ADC1 PowerBrick[0].Chan[0].AdcAmp[2] X9 ADC2 PowerBrick[0].Chan[1].AdcAmp[2] X10 ADC1 PowerBrick[0].Chan[2].AdcAmp[2] X10 ADC2 PowerBrick[0].Chan[3].AdcAmp[2] X11 ADC1 PowerBrick[1].Chan[0].AdcAmp[2] X11 ADC2 PowerBrick[1].Chan[1].AdcAmp[2] X12 ADC1 PowerBrick[1].Chan[2].AdcAmp[2] X12 ADC2 PowerBrick[1].Chan[3].AdcAmp[2] Link to comment Share on other sites More sharing options...
Recommended Posts