Unit101 Posted July 22, 2015 Share Posted July 22, 2015 Recently after update/install of Windows 10 build 10240 the IDE would not do a Build/Download. It would stop with Error MSB4062 and show below complete message: "C:\3_TCIP-Server-RockwellParsing\TCPIP-RockCmdInt-PPmac\TCPIP Server.ppproj(144,5): Error MSB4062: The "PPMAC460CompileTask.CompileTask" task could not be loaded from the assembly C:\Windows\Microsoft.NET\Framework\v3.5\PPMAC460CompileTask.dll. Could not load file or assembly 'file:///C:\Windows\Microsoft.NET\Framework\v3.5\PPMAC460CompileTask.dll' or one of its dependencies. The system cannot find the file specified. Confirm that the declaration is correct, and that the assembly and all its dependencies are available." Appears that something IDE uses related to .NET 3.5 was lost? Fix was to re-run the Patch for the IDE 2-0-3-40. After re-running the patch all was fine. Link to comment Share on other sites More sharing options...
Recommended Posts