michelpizzoto Posted April 7, 2016 Share Posted April 7, 2016 Hi all! I work in Satisloh Company and we use Power PMAC for our VFT machines. I have two brand new CPUs that is not uploading the firmware by USB or SDcard... I think could be a problem with kernel. How can I fix a kernel problem? Which version of Uimage should I use for firmware version 2.0.2.14? Thanks a lot! Link to comment Share on other sites More sharing options...
Jay Lee Posted April 7, 2016 Share Posted April 7, 2016 To uploading the firmware through USB or SDcard, you would need to create a folder in USB flash or SDcard as below: Folder Name: PowerPmacFirmwareInstall Description: Power PMAC firmware will be updated. The installation package "powerpmac.deb" file should be placed in this folder. and you should only use file name as "powerpmac.deb" Please inform us which CPU/form factor you are using. Different CPU will need different firmware. Link to comment Share on other sites More sharing options...
michelpizzoto Posted April 8, 2016 Author Share Posted April 8, 2016 Hi JayL! This is the procedure we do here, but we are having different behavior on each board. One of the CPU don't even blink the USB or SDcard led when they are plugged in, and the other one blink the USB led but don't finish the firmware upgrade. We use CPU EP460C, do you think could be a kernel problem? Regards! Link to comment Share on other sites More sharing options...
steve.milici Posted April 8, 2016 Share Posted April 8, 2016 Capture the boot output on the serial port and send it to support Link to comment Share on other sites More sharing options...
michelpizzoto Posted April 8, 2016 Author Share Posted April 8, 2016 Ok, thanks a lot for your help! Regards! Link to comment Share on other sites More sharing options...
Recommended Posts