JRiemann Posted August 11, 2016 Share Posted August 11, 2016 I have a Power PMAC Clipper which comes with 12-bit analog inputs with -10->+10 V range. I have a sensor that provides a 16-bit analog output with 0-10 V range, which I've connected to 1 of the 12-bit analog inputs on the Clipper. I've having problems with signal noise, which I believe is due to the 12-bit resolution of the analog input. Is there a recommendation to achieve better resolution so I can get the full benefit of the 16-bit analog output? By the way, I'm validating the accuracy/resolution of the 16-bit analog output by using the serial output on the sensor. Perhaps using the serial output is a better option but not sure how I'd integrate that within PMAC. Link to comment Share on other sites More sharing options...
steve.milici Posted August 11, 2016 Share Posted August 11, 2016 The difference in resolution is not an issue as PMAC only sees a 10V signal at its 12 bit resolution regardless of the sensor's resolution. These analog inputs are typically very clean. Make sure your wiring is shielded twisted pair. Also wire the shield drain at the analog input only. What is the serial output protocol? Link to comment Share on other sites More sharing options...
DaveBarnett Posted August 12, 2016 Share Posted August 12, 2016 If your problem really is just 12 bit quantization noise (and not something else), then you might consider using an oversampling/averaging technique. Each doubling of the samples will yield 6db improvement in quantization noise. 'Classic speed/resolution tradeoff applies. see: https://www.silabs.com/Support%20Documents/TechnicalDocs/an118.pdf Link to comment Share on other sites More sharing options...
steve.milici Posted August 12, 2016 Share Posted August 12, 2016 Also note that our 16 bit analog input accessory, ACC-28B, can be used with the Power Clipper. Contact our technical support group for details: support@deltatau.com Link to comment Share on other sites More sharing options...
sdnsdn1234 Posted November 20, 2017 Share Posted November 20, 2017 Connected analog input 0 to 10Vdc to the In put of ADC1. let me know the best interface circuit for external analog input connection to the PMAC ADC Link to comment Share on other sites More sharing options...
steve.milici Posted November 20, 2017 Share Posted November 20, 2017 Connected analog input 0 to 10Vdc to the In put of ADC1. let me know the best interface circuit for external analog input connection to the PMAC ADC You can directly connect to this input. Link to comment Share on other sites More sharing options...
Recommended Posts