cdesilva Posted November 29, 2016 Share Posted November 29, 2016 Hi, All I was trying to follow the discussion thread related to finding the Power PMAC manual/s, but failed to navigate myself. We recently order a Power PMAC with the following specifications. Part #: PBC4-G21-000-A000000 4 Axes Power Brick Controller 800MHz EP460EX CPU 2 GB RAM 1 GB Flash/SD-Card No Additional Ethernet/EtherCAT option Axes 1-4 True 16-bit DAC - 4 Encoder and Flag Inputs with 32/16 Digital I/O No Analog Feedback Interface No Special Serial Feedback CONKIT-P-1C-A -> Included Below is my question. I would like to know what is the maximum clock frequency of encoder signals this PMAC can handle? If you could point me to the manual and where in the manual I can find this information that would be very helpful. Chanaka De Silva NSLSII controls Link to comment Share on other sites More sharing options...
cdesilva Posted November 30, 2016 Author Share Posted November 30, 2016 I was able to find the documentation. Thanks Chanaka Link to comment Share on other sites More sharing options...
Recommended Posts