terrydeltasigmacorp.com Posted January 31, 2017 Share Posted January 31, 2017 I need the address of the Control Register of a ACC14E and a description of the register to define inputs and outputs. The manual does not include info for Power PMAC. Link to comment Share on other sites More sharing options...
steve.milici Posted February 1, 2017 Share Posted February 1, 2017 The manual for the ACC-14E is currently under modification and should be updated soon. It uses similar structure elements as the ACC-65E, 66E, 67E and 68E as specified in the manuals for these keeping in mind that you use ACC14E[n] instead of ACC65E[n] and ACC14E[n].CtrlReg has greater flexibility. Link to comment Share on other sites More sharing options...
terrydeltasigmacorp.com Posted March 2, 2017 Author Share Posted March 2, 2017 Can you tell me what the power capabilities of the outputs of the ACC-14E are? I need to drive a 50 Ohm input with one of the outputs. I cannot find the power info in the manual for the outputs individually. Can it drive the 100mA required for driving a 50 Ohm input. Thanks Link to comment Share on other sites More sharing options...
steve.milici Posted March 3, 2017 Share Posted March 3, 2017 The outputs are TTL with 3.3K pull-up resistors. This will severely reduce the "high" level. Link to comment Share on other sites More sharing options...
Recommended Posts