fatihbeyy Posted May 9, 2017 Share Posted May 9, 2017 PowerPmac ide version 2.2.1.25 Firmware version 2.3.1.0 Compile Error What can be the problem ------ Build started: Project: PowerPmac5(192.168.1.125:arm,LS1021A-usermode), Configuration: Debug Any CPU ------ Please wait while mapping Power PMAC variables. End of syncing the database. PMAC variables are mapped successfully. Build Process For capp1.out has started. C:\Users\NacioOo\AppData\Local\Temp\h0fxxs2c.fnq\Temp\PowerPmac5.ppproj(0,0): Error : /usr/local/lib/gcc/arm-omron-linux-gnueabihf/4.6.4/../../../../arm-omron-linux-gnueabihf/bin/ld: cannot find -lpthread_rt C:\Users\NacioOo\AppData\Local\Temp\h0fxxs2c.fnq\Temp\PowerPmac5.ppproj(0,0): Error : /usr/local/lib/gcc/arm-omron-linux-gnueabihf/4.6.4/../../../../arm-omron-linux-gnueabihf/bin/ld: cannot find -lxenomai C:\Users\NacioOo\AppData\Local\Temp\h0fxxs2c.fnq\Temp\PowerPmac5.ppproj(0,0): Error : collect2: ld returned 1 exit status Build Process For capp1.out has ended. Done building project "PowerPmac5.ppproj" -- FAILED. Build FAILED. Project Building and Mapping total time = 1.343 sec ========== Build: 0 succeeded or up-to-date, 1 failed, 0 skipped ========== Link to comment Share on other sites More sharing options...
steve.milici Posted May 10, 2017 Share Posted May 10, 2017 I think this is a library issue. At this path, "C:\DeltaTau\Power PMAC IDE\Compilers\usr\local\dtlibs", delete everything except for the "Default Libraries" folder. Then "unload/reload & clean" the project and then rebuild the project. Link to comment Share on other sites More sharing options...
GodPLC Posted June 20, 2017 Share Posted June 20, 2017 I think this is a library issue. At this path, "C:\DeltaTau\Power PMAC IDE\Compilers\usr\local\dtlibs", delete everything except for the "Default Libraries" folder. Then "unload/reload & clean" the project and then rebuild the project. Hi Steve, I have tested on your suggestion and keep getting the same issue. This issue happen when I Uninstall IDE 3.0.0.2 and reinstall 2.2.0.29 Link to comment Share on other sites More sharing options...
steve.milici Posted June 20, 2017 Share Posted June 20, 2017 I think this is a library issue. At this path, "C:\DeltaTau\Power PMAC IDE\Compilers\usr\local\dtlibs", delete everything except for the "Default Libraries" folder. Then "unload/reload & clean" the project and then rebuild the project. Hi Steve, I have tested on your suggestion and keep getting the same issue. This issue happen when I Uninstall IDE 3.0.0.2 and reinstall 2.2.0.29 Make sure to install the patch to 2.2.1.25. Link to comment Share on other sites More sharing options...
GodPLC Posted June 21, 2017 Share Posted June 21, 2017 Hi Steve, I upgrade to 2.2.1.25 and still having the same issue. If I don't clean and rebuild, I got this: Please wait while mapping Power PMAC variables. End of syncing the database. PMAC variables are mapped successfully. Build Process For capp1.out has started. C:\Users\*******\Documents\PowerPmacSuite\PowerPmacPOC\GcodeServo3\GcodeServo3\C Language\Background Programs\capp1\capp1.c(1,0): Error : gplib.h Build Process For capp1.out has ended. Done building project "GcodeServo3.ppproj" -- FAILED. Build FAILED. Project Building and Mapping total time = 0.297 sec Link to comment Share on other sites More sharing options...
steve.milici Posted June 21, 2017 Share Posted June 21, 2017 Please contact support@deltatau.com and send the project as a zip file renamed to ".zzz". Link to comment Share on other sites More sharing options...
GodPLC Posted June 22, 2017 Share Posted June 22, 2017 Please contact support@deltatau.com and send the project as a zip file renamed to ".zzz". I don't think is the project file having the issue, it the software after downgrade. I try using another PC, Windows 7 installing for the 1st time and no issue build and download. Link to comment Share on other sites More sharing options...
Recommended Posts