jtaseff Posted May 17, 2017 Share Posted May 17, 2017 Trying to get a homing search move to work for an incremental encoder. I have Motor[2].HomeOffset=0. I run #2home, it does the homing search. It's set to capture on the Home flag, which works, and the Motor[2].HomeInProgress changes to HomeComplete. However, when this happens, the motor position gets set to -5,000,000ish counts and it tries to post-trigger-move to position 0, which is outside of travel. What am I doing wrong that when it sees the home flag, the position gets set to a non-zero value? I have a 2nd identical motor configured exactly the same which works as expected - the position at the home flag gets set as the 0 point and it stops moving. Link to comment Share on other sites More sharing options...
Omron Forums Support Posted May 18, 2017 Share Posted May 18, 2017 Where or what parameter gets set to -5,000,000ish? Are there any PLCs running, such that might cause this? Link to comment Share on other sites More sharing options...
jtaseff Posted May 18, 2017 Author Share Posted May 18, 2017 The motor position shown in the position watch window jumps to that count. I can j=-5,000,000 and it will jog to that spot where it finds the home flag. After powering on today, the position that it picks up at the home flag is now -12,000,000ish instead of -5,000,000ish, at the same physical location. Nothing running at all except me typing #2home in the terminal. Link to comment Share on other sites More sharing options...
Alex Anikstein Posted May 18, 2017 Share Posted May 18, 2017 Can you post a screen shot of the IDE after issuing the home command? Preferably showing the Position Watch Window, the Terminal Window, and the Motor Status Window. Link to comment Share on other sites More sharing options...
jtaseff Posted May 18, 2017 Author Share Posted May 18, 2017 Screenshot is attached, and a listing of backup Motor[2], backup EncTable[2], and gate3[0].chan[1]. I can't see anything different between motors 2 and 3. Did #2home, then stopped it with #2jog/ after I saw HomeComplete to keep it from running into the hard stop when it tries to post-trigger-move to 0. The position shown is where I expect 0 to be. Then did #3home, and it stopped happily at 0 at the home flag as expected. No kinematics, just have #2->100000ybackup.txt Link to comment Share on other sites More sharing options...
Recommended Posts