beheredurgesh Posted July 24, 2017 Share Posted July 24, 2017 Dear Sir, We are using ACC 84 E with Turbo UMAC. In the RACK we have only 2 Accessories 1. ACC 24E2A & ACC 84 E. Switch Setting on ACC 84 E is Sw1 ON/ 2,3,4, OFF and encoder connected to Channel 1 So the address is $78d00. We are using 22 Bit SSI GERY code Single turn encoder. Encoder Voltage is 24 V. 24 V is connected to encoder directly. 24vGnd is connected to GND of encoder & Pin no 5 of D connector. As per manual we have done the following settings with Technique 3 ( as encoder is Greater than 19 bit) In encoder conversion table we have done following entries. Entry 5 Conversion Type -> Parallel position from Y word with no filtering. Source Add-> $78D00 Witdth in Bits-> 22 Offset - > 0 Normal shifting. We have assigned $3506 to I103 & I104 As per manual we have set i108=1 and i109=1. But we are not getting any feedback. This encoder works with ACC 53E. Link to comment Share on other sites More sharing options...
Omron Forums Support Posted July 25, 2017 Share Posted July 25, 2017 According to the ACC-84E manual, Y:$78D00 is 1 Off, all else on. Are you sure you don't have this backwards? Link to comment Share on other sites More sharing options...
Recommended Posts