Unit101 Posted November 22, 2017 Share Posted November 22, 2017 Since using IDE 3.1.1.0 working with a CK3E, when connecting it tells me there is NO Project in PMAC... however this is not true. All starts and works fine... Is it just me ? bigcat Link to comment Share on other sites More sharing options...
navinvinayan Posted November 28, 2017 Share Posted November 28, 2017 hi, while i was saving my project inside ck3e, power went suddenly, which caused ck3e to show no project message.Even after rebooting/resetting ck3e the situation was same.So we opted for a new controller assuming that ,the flash memory of the ck3e controller is gone. Link to comment Share on other sites More sharing options...
Unit101 Posted November 28, 2017 Author Share Posted November 28, 2017 Interesting.... mine is working fine, project is loaded and boots ok. ONLY when starting IDE is says "no project in pmac" ... which is not true... IDE is missing something... I just OK and go on... no problems. Just started with CK3E older fware and new IDE Link to comment Share on other sites More sharing options...
Omron Forums Support Posted November 28, 2017 Share Posted November 28, 2017 Mike: I don't see that pop-up. Just to be sure I turned off my ck3e, closed the ide, turned on my ck3e and then opened the ide. Do you actually have a project, or just ENI and config files? Navin: If you can still talk to linux (ping or putty) I would try the "PowerPmacFirmwareInstall" folder before giving up on the flash memory. Link to comment Share on other sites More sharing options...
navinvinayan Posted November 30, 2017 Share Posted November 30, 2017 Hi Eric Hotchkiss , i tried a firmwire install ,but still the problem was persisting at that time.Even the 'save' command was not issuing in the ck3e controller.Is there any other method than firmware installation? And what do you mean by 'powerpmacfirmwareinstall' folder. Link to comment Share on other sites More sharing options...
Unit101 Posted November 30, 2017 Author Share Posted November 30, 2017 Mike: I don't see that pop-up. Just to be sure I turned off my ck3e, closed the ide, turned on my ck3e and then opened the ide. Do you actually have a project, or just ENI and config files? Yes there is a project running in the pmac, the machine is actually powered up and running the machine when I connect from IDE... so the PMAC is running a machine including Ecat and I connect with IDE and it says No Project in PMAC... it does not cause any issue, but for sure this is related to latest IDE... I'll test some more and see if can reproduce on a different PMAC setup... since not causing a issue I've not spent much time on this... just keep an eye out and I posted because I wondered if anyone else seen this??? Thanks Navin: If you can still talk to linux (ping or putty) I would try the "PowerPmacFirmwareInstall" folder before giving up on the flash memory. Link to comment Share on other sites More sharing options...
Recommended Posts