piefum Posted January 19, 2018 Share Posted January 19, 2018 Hi all I have some strange issue via some ethercat IO terminals. This is my setup: PowerBrick LV (version IMS), 8 axis ethercat IO license Ethercat Terminals connected: - EK1100 - 3x EL 5032 (2 channel Endat 2.2 input) - 1x EL3508 (8 channel RTD input) I setup the system using the PMAC IDE 2.2.1.25. I tested the system with only the EL5032: I put the 6 readings from the three EL5032 in the foreground task, and that worked fine. I added in a second moment the EL3508 to gather some PT100. I added to the chain, re-performed the ethercat configuration, and added the RTD values to the foreground task together with the other variables. What I got is the EL3508 that does not exit the PREOP mode, and consequently the variables are not updated in the foreground task. The strange thing is that if I perform the reading of the register of the EL3508 via terminal with the command: ethercat -m0 -p4 -t int16 upload 0x6000 0x11 I can correctly see the values of the PT100. So, the question is: how is it possible that the foreground task is not able to get the same register values that I can read via the terminal? thanks a lot Bests gigi Link to comment Share on other sites More sharing options...
Recommended Posts