Jump to content
OMRON Forums

PMAC IDE Question


Recommended Posts

Hello,

 

I am running a program which gathers data through the Delta Tau Plot feature. Once I upload the data, I made a plot of motor(1) Actual position and motor(1) cmd position on the left axis and time on the horizontal axis. When I save the data into a .txt file, the file gives a list like:

 

Time(sec) Motor[1] Act Position Motor[1]CmdPosition

0.00000000000000000 -1806515.47722567000000000 -1806520.06591749000000000

0.00250000000000000 -1806519.47722567000000000 -1806520.06591749000000000

0.00500000000000000 -1806519.47722567000000000 -1806520.06591749000000000

0.00750000000000000 -1806517.47722567000000000 -1806520.06591749000000000

0.01000000000000000 -1806520.47722567000000000 -1806520.06591749000000000

 

Can someone please explain what units the actual and command position are in?

 

Thanks,

Matt

Link to comment
Share on other sites

  • Replies 1
  • Created
  • Last Reply

Top Posters In This Topic

Guest
This topic is now closed to further replies.

×
×
  • Create New...