hannsx Posted July 20, 2018 Share Posted July 20, 2018 Hi, in the User Manual it says that I can not use float variables or math in the ISR. So is it not even possible to declare a float pointer and to do a typecast of an integer value to write it to that pointer? I would like to use the speed of the ISR to inject a position offset and would therefore need to write to the floating point register Motor[x].CompPos. Ii know that injecting a position offset is possible by using a 0D-Compensation Table, but is there a way to accomplish what I have in my mind? I am using a Linear Motor on a PowerbrickLV, best regards, hannsx Link to comment Share on other sites More sharing options...
hannsx Posted July 20, 2018 Author Share Posted July 20, 2018 I got the advice from the support to realize my application in either the servo or phase interrupt, as there are no benefits from having position corrections faster than these. In these Interrupts there are no Limitations to the data formats, best regards, hannsx Link to comment Share on other sites More sharing options...
Recommended Posts