kandauru Posted July 25, 2018 Share Posted July 25, 2018 Hi, we have upgraded our system with CK3M controller (previously we had Power Brick controller). The main problem is that we have to tune all motors again, but they are same, why?. All parameters (Kp, Kd, Kvff and others) were dramatically changed. Kp parameter looks limited to 4-7. if I try to increase it, the plot gets very strange shape. A new UI for tuning motors (I use Power PMAC IDE 4)does not work! Basic tuning feature starts running, but never stops. Our problem - we cannot reach same behavior of motors with Kp=4. Is there something "undocumented"? Link to comment Share on other sites More sharing options...
Faraday MC - Tony Posted July 26, 2018 Share Posted July 26, 2018 I had problems with plotting and tuning because the Windows 10 firewall blocked the DeltaTauGatherProgram. Once I allowed it through the firewall everything worked. Did you have the filtered PWM or true DAC outputs on your Power Brick Controller and what do you have on the CK3M? The gains will be different if you change between the two types. Link to comment Share on other sites More sharing options...
Alex Anikstein Posted July 26, 2018 Share Posted July 26, 2018 Also, are the clock settings the same (Gate3[0].PhaseFreq/Gate3[0].ServoClockDiv)? That's the other big "non-tuning related" thing that has a large impact on tuning. Link to comment Share on other sites More sharing options...
kandauru Posted July 30, 2018 Author Share Posted July 30, 2018 What should be Gate3[x].DacStrobe parameter for CK3M? Link to comment Share on other sites More sharing options...
kandauru Posted July 30, 2018 Author Share Posted July 30, 2018 I had problems with plotting and tuning because the Windows 10 firewall blocked the DeltaTauGatherProgram. Once I allowed it through the firewall everything worked. Did you have the filtered PWM or true DAC outputs on your Power Brick Controller and what do you have on the CK3M? The gains will be different if you change between the two types. We have true DAC outputs on all our controllers. Link to comment Share on other sites More sharing options...
kandauru Posted August 3, 2018 Author Share Posted August 3, 2018 Hi again, there are 3 motors connected to same Gate3[0]. From Power PMAC IDE, I enable one of them and jog it, everything is good, if I enable any other motor and jog the same motor, the strange noise is coming from the motor. ( in both directions ). It happens like this with two others too. We have have checked electrical wiring and found that it is OK. Any idea why it might happen? Thank you in advance. Link to comment Share on other sites More sharing options...
Sangmo Posted August 24, 2018 Share Posted August 24, 2018 Hi again, there are 3 motors connected to same Gate3[0]. From Power PMAC IDE, I enable one of them and jog it, everything is good, if I enable any other motor and jog the same motor, the strange noise is coming from the motor. ( in both directions ). It happens like this with two others too. We have have checked electrical wiring and found that it is OK. Any idea why it might happen? Thank you in advance. If you don't need to change the DAC Strobe when using CK3M, you can use the default value. You should check the Gate3.Chan[j].CountError to see if the feedback signal is disturbed. Link to comment Share on other sites More sharing options...
Recommended Posts