wlewis Posted December 20, 2018 Share Posted December 20, 2018 We have a PowerPMAC with a single MACRO station connected to it. When I issue a 'macroringorderbackup' command, followed by a 'save', a new 'bkupring0stn1.cfg' file is generated in /opt/ppmac/usrflash/Project/Configuration. Two questions: - is there a way of having this file automatically uploaded to the IDE project in the same way that the pp_save.cfg and pp_custom_save.cfg files are uploaded? - is there another way of backing up the MACRO station to the PowerPMAC? I ask this because if I set the MACRO station number to something like 28 (i.e., not the number assigned by the 'macroringorderinit' command) then the 'macroringorder...' commands no longer see the MACRO station. Or am I doing something wrong on the MACRO master in the PowerPMAC in this situation? Thanks, Wayne Link to comment Share on other sites More sharing options...
Recommended Posts