rvanderbijl Posted March 13, 2019 Share Posted March 13, 2019 We're using a Power PMAC 465 CPU with the Etherlab EtherCAT stack. The system wasn't running much last night (aside from EtherCAT with one device), and when I looked at the system this morning, it was frozen and the IDE (4, latest) had lost connection to the PMAC. The serial console showed the following: ecm0: BUG! Tx Ring full when queue awake! ecm0: BUG! Tx Ring full when queue awake! ecm0: BUG! Tx Ring full when queue awake! ecm0: BUG! Tx Ring full when queue awake! ecm0: BUG! Tx Ring full wh And yes, the last line was literally cut off like that (guess that's when it crashed). Firmware 2.4.0.180. Any suggestions? Link to comment Share on other sites More sharing options...
steve.milici Posted March 13, 2019 Share Posted March 13, 2019 This would be a technical support issue. Please contact ODT's technical support with a full serial port boot response: support@deltatau.com Link to comment Share on other sites More sharing options...
Recommended Posts