dholden Posted April 9, 2019 Share Posted April 9, 2019 I have an ACC-5E that was working fine with a Power PMAC but when i try to use it with a Turbo PMAC it does not accept configuration. Specifically when using the card in a rack system with a Trubo PMAC i cannot set any of the MACRO variables, for example: I6800=6527 I6802=3 I6840=$4030 I6890=$90 etc... When setting a value to these variables they simply return to a value of zero. Any idea why this would be the case? is there a difference between the Power PMAC card vs the Turbo PMAC card? Are there jumpers that need to be changed Any Ideas or suggestions would be appreciated Thanks Link to comment Share on other sites More sharing options...
steve.milici Posted April 9, 2019 Share Posted April 9, 2019 Verify the card is addresses as the first MACRO IC. Also verify there is no other MACRO IC card at this address. Link to comment Share on other sites More sharing options...
dholden Posted April 10, 2019 Author Share Posted April 10, 2019 S1 Dipswitch are all set to "on" This should make the base channel address $78400 (MARCO IC 0) This is the only other card in the rack right now (with the Turbo PMAC CPU) to help with troubleshooting Also, I can confirm that J1 jumper pins 1-2. I am using fiber for MACRO not the RJ45 connectors. Link to comment Share on other sites More sharing options...
steve.milici Posted April 15, 2019 Share Posted April 15, 2019 This would be a technical support issue. Please contact ODT's technical support at: support@deltatau.com Link to comment Share on other sites More sharing options...
Recommended Posts