Jump to content
OMRON Forums

Halted program resumes with feed-rate change


paddax
 Share

Recommended Posts

The manual states

 

The h command is very similar in effect to a %0 command, except that deceleration and subsequent re-acceleration are controlled by Coord[x].FeedHoldSlew, not by Coord[x].TimeBaseSlew. Also, execution can be resumed with an R or S command, instead of a %100 command. In addition h works under external time base, whereas a %0 command does not.

 

I've found to my embarrassment and luckily no one's health that issuing "%100" when halted resumed the program execution.

 

CPU: PowerPC,460EX

VERS: 2.4.0.180

 

The desired functionality is when an event occurs the system should halt until the condition is cleared, the way I've implemented this is to prevent R and S commands during this phase. Is there a simple method of preventing execution in a modal manner.