Jump to content
OMRON Forums

Recommended Posts

Posted
I connected a Renishaw 26-bit BiSS-C encoder to the PMAC and I'm monitoring the two encoder signals with a oscope. In PEWIN the Cts Per Unit is set to 1, and the position shows 107500. On the oscope it shows 631787 (26-bit position only, status and CRC bits removed). The waveform format is exactly as defined in the BiSS-C protocol, and CRC is correct, so I assume there's no error/noise causing measuring problem. Then how could the two readings be so different? Is the position window in PEWIN showing the raw read back value from the encoder?
  • Replies 1
  • Created
  • Last Reply

Top Posters In This Topic

Top Posters In This Topic

Guest
This topic is now closed to further replies.

×
×
  • Create New...