Jump to content
OMRON Forums

ACCE1 Power Capacity


cryovolcano

Recommended Posts

  • Replies 1
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

The ACC-E1 has the following specifications:

+5V @ 14A

+15V @ 1.5A

-15V @ 1.5A

 

It could be possible with that “load” of cards the ACC-E1 is compromised but the total of the cards listed are well within the specification above:

Power UMAC 465 CPU @3.0A

4 x ACC24E3 @1.5A = 6.0A

2 x ACC84E @0.36A = 0.72A

1 x ACC72EX @1.0A = 1.0A

2 x ACC65E @0.38A = 0.76A

 

What issues are you seeing?

 

Note that the UMAC backplane has separate terminals for an external PS.

Link to comment
Share on other sites

Guest
This topic is now closed to further replies.

×
×
  • Create New...