brinj Posted October 18, 2019 Share Posted October 18, 2019 At some point since 2009 the GeoBrick Default I7m03 changed from 1234 to 2257. I understand that this was for reasons of limiting either the maximum ADC or DAC frequency. I have recently used a 1A geobrick variant and selected the recommended 40kHz PWM frequency , but at this rate the ADC values as read by Mxx05 are random and range from zero to full scale, even without motor power. If I reduce the ADC clock divider from 3 to 2 this reading becomes stable , but I want to be sure I don't exceed the new maximum allowable settings. Does anyone on here know what the maximum allowable settings are for the hardware clock settings of an 8 channel 1A/3A geobrick LV running at 210MHz. ( avoiding 240 just in case we have some older hardware that predates the wait states firmware fix) Thanks in advance Link to comment Share on other sites More sharing options...
Recommended Posts