jbeasley Posted November 7, 2019 Share Posted November 7, 2019 System is PowerBrickLV, 8 Channel 5/15 Amp. So I have built a new milling table system and tested it with fully closed loop BLDC Motors and stepper motors. Both systems worked as expected once tuned and programmed. One issue i seem to have with the stepper motor configuration is if I do a reset and save with $$$***, save. Then download my fully working project the motors won't move. I just see a following error develop. If I open the System -> Motors -> 1-5 one at a time and change one thing, for example change my input Voltage by 1 V, and step through each configuration step for the motor saving it and commissioning. Then I download my working configuration everything works fine? I even tried copying the entire systemsetup.cfg to a Global include to force all the parameters back to my working config and it still won't move the motors until I step back through the Motor Setup even though they all show Green and good to go. What variable is getting set to enable the direct micro-stepping that i can't seem to set from a text configuration? Shouldn't I in practice be able to forgo all the GUI system setup options and just pipe in a hard-coded system configuration as a Global include Starting out with sys.WpKey=$AAAAAAAA then save and Comment out the contents of that file and continue with the rest of my programming. Then once everything is tuned and working perfect I can create a new master configuration file from the systemsetup.cfg and make that my fail-safe to reload in the even something gets horribly out of wack? Thanks John. Link to comment Share on other sites More sharing options...
Recommended Posts