biscchr Posted July 9, 2020 Share Posted July 9, 2020 Hi, I am working with an CK3E ARM PowerPMAC running FW 2.5.4.0. For integrating our own custom service, I was trying to use init.d for running the service at startup. Unfortunately, when running update-rc.d the whole init.d structure gets messed up. After that, a lot of services get started, that bring error messages in the console (samba, winbnd, etc.). Event if I don't add a new service on a plane .vhd image, I get these error messages during boot after simply running update-rc.d. Additionally there are more services starting than before running update-rc.d. So my question is: Why is update-rc.d messing up the startup sequence and how can I fix that? How can I add a new service to the startup procedure without using update-rc.d? Best, Christopher Link to comment Share on other sites More sharing options...
Omron Forums Support Posted July 9, 2020 Share Posted July 9, 2020 You should be able to add your startup script to "/.readonly/etc/init.d" and then place symbolic links in "/.readonly/etc/rc2.d/SXXntp" following the already existing naming conventions and using the number in the name to determine run order. Don't run update-rc.d. Link to comment Share on other sites More sharing options...
Recommended Posts