GustavoGS Posted August 20, 2020 Share Posted August 20, 2020 Hello all, I would like to know if it is possible to control 3-phase stepper motors using Power Brick LV. The Power Brick LV User Manual shows motor wiring for 2-phase stepper motors and 3-phase brushless servo motors only. Can 3-phase stepper be wired the same as 3-phase brushless servo? Also according to the Power Brick LV User Manual: "BrickLV.Chan[j].TwoPhaseMode selects the operational output mode of the amplifier channel. If set to its default value of 0, the amplifier is set to 3-phase operational mode, using the U, V, and W output lines. This operational mode is mainly used with Y-wound or delta-wound brushless servo motors (but 3-phase stepper motors do exist)." At first, my idea was to set TwoPhaseMode = 0 and try driving the motor using the brushless motor setup. Link to comment Share on other sites More sharing options...
Omron Forums Support Posted August 20, 2020 Share Posted August 20, 2020 Are you intending to use the encoder or not? If not it would be best to start with the "Stepper Motors – Direct Microstepping without Encoder" example, but will the following changes: BrickLV.Chan[].TwoPhaseMode=0 Motor[].PhaseOffset = 683 Motor[].PhaseMode = 0 I2T Protection would already be correct for a 3 phase motor in that section, but once it's updated to be correct for 2 phase you'll want to keep the cos(30) like below: Motor[].MaxDac/I2tSet = PeakCurrentrms * 32768 * √2 * cos(30°) / MaxAdc Link to comment Share on other sites More sharing options...
Recommended Posts