wonjae lee Posted March 1, 2022 Share Posted March 1, 2022 (edited) Hello. I"m Using Power PMac(UMac) I Have a program NC-code witch has three sub-programs. sub prog size is 1. 2 MB, 2. 80 MB, 3. 100 MB, each. The Problem is... It takes a lot of time for downloading sub prog. and my PMac's memory amount is only 320 MB. so i can not use sub=prog that size exceed over 300 MB(aprox) is there anyway to run program directly from usb memory or hdd of PC? Like Fanuc Controller SYstem? or Using Rotary Buffer is the only way to solve this program? If anyone has same issue of me, or know the answer about this. Please Answer me. Thanks. Edited March 1, 2022 by wonjae lee Quote Link to comment Share on other sites More sharing options...
zerbzhang Posted March 3, 2022 Share Posted March 3, 2022 In the c language project, add the reading program, use the PMAC_linux command to load the NC program, and realize the NC program you need to dynamically load the usb. Quote Link to comment Share on other sites More sharing options...
wbzhong Posted March 12, 2022 Share Posted March 12, 2022 Hi, you can upload the NC file to the PMAC with a FTP client (e.g. FileZilla). The destination folder should be in /var/ftp/usrflash/. Then, issue the following command to ininitialize the sub prog: // No space between -i and /var gpascii -i/var/ftp/usrflash/Temp/mysubprog.nc And don't forget to enclose the subprog code in the following structure: open subprog xxx <subprog code> return close Quote Link to comment Share on other sites More sharing options...
wonjae lee Posted August 11, 2022 Author Share Posted August 11, 2022 On 3/3/2022 at 2:58 PM, zerbzhang said: In the c language project, add the reading program, use the PMAC_linux command to load the NC program, and realize the NC program you need to dynamically load the usb. is there any smaple code i can get? if any, let me know please. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.