Omron Forums Support Posted March 7, 2022 Share Posted March 7, 2022 Introduction Purpose: How to wire a momentary switch to unlatch an output.Explanation: The MS-Connect 210 does not allow the external membrane switches to be programmed for other uses. In order to unlatch an output, you will need to wire a separate momentary switch to “Input 1” on the inside terminal(s) of the MS-Connect 210.Supported Products: • All readers that allow Output X = Latch mode 1 (unlatch on Input # 1 pin) where X is the number of the Output in the I/O section of the reader settings. Typically called Output 1, 2, or 3. Here is a quick sketch showing the wiring of a switch to the terminals in the MS-Connect 210 The connections are as follows: PWR+ to INPUT1+ PWR- to one side of the switch INPUT1- to the other side of the switch You may be able to remove one of the feed-throughs on the bottom of the MS-Connect 210 and install the switch in the opening to avoid having to run cable. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.