Code Reading
197 topics in this forum
-
- 0 replies
- 108 views
This describes how to wire in a momentary contact switch to the Input of the scanner for such things as unlatching output's. kA23800000008KHCAY_en_US_1.pdf
Last reply by Omron Forums Support, -
Reference the HawkEye 1500 Verification Manual for a list of parameters that are measured for each verification type. The verification manual is part of the manual set downloaded and installed with the ReadRunner 2.4.1 and is accessible from the Start menu. The manual is also available in the download center: http://files.microscan.com/elqNow/elqRedir.htm?ref=http://files.microscan.com/_att/68d53eb8-fac9-4061-8382-9d14ec80534c/hawkeye1500manuals.zip
Last reply by Omron Forums Support, -
- 0 replies
- 27 views
Simple wiring diagram for wiring outputs to the 5V TTL signals in the MS-3. The MS-3 can Sink up to 10mA and source up to 2mA.
Last reply by Omron Forums Support, -
- 0 replies
- 31 views
Simple wiring diagram for wiring outputs to the 5V TTL signals in the MS-4/Quadrus Mini Family of products. The Mini's can Sink up to 10mA and source up to 10mA. kA23800000008IvCAI_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 39 views
This document describes the revised pin assignment for Connector T on the QX-870 and QX-1. It also provides a list of new part numbers for the affected devices.
Last reply by Omron Forums Support, -
- 0 replies
- 35 views
This document describes X-Mode functionality in relation to the MINI Hawk Imager. kA23800000008IOCAY_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 38 views
This information is for all versions of MS-4, Quadrus MINI and MINI Hawk. Models with Standard IP mode only Firmware #35-634001-24 and older has Pharmacode. Firmware #35-634001-25 and later, no Pharmacode installed. To add Pharmacode, downgrade firmware to -24 using the attached file. Models with Standard and Q-mode Image Processing modes Firmware #35-634001-24 or older has Pharmacode in Q-mode and Standard Image Processing modes. Firmware #35-634001- 25 and later has pharmacode in Q-mode. X-mode Pharmacode works in all revisions. kA23800000008GDCAY_en_US_1.mot
Last reply by Omron Forums Support, -
- 0 replies
- 34 views
Use a mirror that reflects off the first surface, not the back. This will reduce distortion of the image. use a material that will reflect as much light as possible to maximize the light signal of the symbol. Glass shoudl be defect-free to prevent distortion.
Last reply by Omron Forums Support, -
- 0 replies
- 39 views
Solution is to upgrade customer to 3.7.2 or later - this contains code that fixes the problem. In more detail, the problem was that the camdef file stored with the job in flash on the HE1600T camera gets corrupted or lost. When the job loads it can't find the camdef and the camera then crashes. In 3.7.2 the camdefs are all stored in the firmware and then moved into memory at boot time before the job loads. This prevents the problem from crashing the camera.
Last reply by Omron Forums Support, -
Because WebLink for MicroHAWK ID-series barcode readers is web-based and is accessed via the reader's IP address, it only works over Ethernet connections. This may be an emulated Ethernet connection over USB (ID-20 or ID-30 with USB adapter cable) or over a native Ethernet connection (ID-40). It CANNOT be accessed over RS-232. If RS-232 communication is required for the application, configuration must be done using our ESP software. Software Version WebLink Operating System Any
Last reply by Omron Forums Support, -
If a data string message of "scan sync not present" is output by your laser barcode scanner, this indicates a developing mirror motor hardware failure and the unit should be returned to OMRON Microscan Systems for repair.
Last reply by Omron Forums Support, -
- 0 replies
- 57 views
This document describes symbol reconstruction methodologies in the QX-830 and QX-870. kA23800000008I9CAI_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 25 views
Summary Tests were run using an ID-20 and a Raspberry Pi3 SBC running Raspbian to determine to what extent the ID-20 is compatible with this hardware / software combination. It was found that, if the ID-20 has a static IP address, then WebLink and Telnet can both be used to talk to the reader. However, the virtual com port cannot be accessed from Linux Initial Network Configuration 1. Starting with a clean Raspbian operating system. Set up your wifi or wired network for internet access if required. 2. Go to network icon in top-right of menu bar and right-click on it. 3. You'll see two network adapters listed if you click on the interface drop-down …
Last reply by Omron Forums Support, -
- 0 replies
- 35 views
This example application will use one MS-3 to scan a carton, then teach the product code to the product scanner. If the product is incorrect, the output will fire. The Ms-Connect 210 is used as the intermediate device to control the two scanners. The carton scanner will strip off the first two and last one digits from the carton (ITF) code, and load it into the product scanner, which will then scan the UPC codes. kA23800000008E7CAI_en_US_1.zip
Last reply by Omron Forums Support, -
- 0 replies
- 38 views
Using a DELL laptop with Nvidia Quadro 880M, locate and capture/decode buttons cause the video driver to crash, occasionally causing a blue screen. Updating drivers to 260.99 resolved the problem.
Last reply by Omron Forums Support, -
- 0 replies
- 33 views
This Link is to a YouTube video showing the addition of the QX-800 series to an EIP Network. http://www.youtube.com/watch?v=7TJIcevRIjo
Last reply by Omron Forums Support, -
- 0 replies
- 29 views
Download and install the current QX Hawk firmware to add the improved Ethernet IP interface. http://files.microscan.com/elqNow/elqRedir.htm?ref=http://files.microscan.com/_att/d46296e3-3002-4189-9839-e7516e4e6fbb/QX_Hawk_FW_APP-15_DSP-11.zip
Last reply by Omron Forums Support, -
- 0 replies
- 44 views
How to update the QX-hawk firmware when the unit does not respond to the normal auto connect. 1. Start the QX-Hawk in Safe mode. To do this , power the unit while keeping the Default pin (3) connected to the ground pin (7). In the standard QX cables, these are the green and blue wires. Keep the connection until the red cross comes on or for about 15 seconds. 2. Start ESP and force connect with communication settings 115,N,8,1. 3. Go to the ESP terminal. 4. Type and see if there is an answer. The unit should respond with the firmware versions and the text SAFE MODE. 5. Try to update the APP code which has been working before. The update can take more than 10 minutes. After…
Last reply by Omron Forums Support, -
- 0 replies
- 33 views
Every symbol decoded will run through the database. - If the symbol is in the database, it is a Match. - If the symbol is not in the database, it is a Mismatch. At the end of the read cycle, there is only ONE result, which will be (in the order of priority): - If ANY symbols are not decoded (the number of symbols required is set in the Multisymbol option, under Read Cycle), the read cycle result is Noread. - If ANY symbols do not match the database, the result is Mismatch. - If ALL symbols are decoded, and they are in the database, the result is Match. Each of the three outputs can be programmed for one of these events, and in some cases, a combination of these events. Al…
Last reply by Omron Forums Support, -
- 0 replies
- 45 views
This setup is very Generic and assumes you are in early setup stages with control of placement of a trigger and if possible line speed. The note shows examples and uses of some parameters to help in most moving based issues. This best case scenario has the barcode directly under the Imager, in Field Of View, when the trigger goes active. kA23800000008KOCAY_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 23 views
The recommend torque for the front panel accessory screws is 2 in-lbs; and 8 in-lbs for the mounting plate screws.
Last reply by Omron Forums Support, -
- 0 replies
- 25 views
The attached universal mounting spec sheet is for the following products: MS-880/MS-890 (for MS-890, reference MS-880) MS-3 Laser/CCD MS-2 (reference MS-3) MS-820 MS-860 MS-9 QX-830 (reference MS-820) QX-870 (reference MS-860) MS-850 (reference MS-860) MS-4/Quadrus MINI series kA23800000008EmCAI_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 41 views
Attached to this article is a step by step guide for settings up MicroHAWK ID readers as well as Microhawk MV cameras to send FTP images directly to a server. The document describes the setup on the server side using Filezilla, as well as setup on the reader / smart camera. kA23800000007nnCAA_en_US_1.docx
Last reply by Omron Forums Support, -
- 0 replies
- 37 views
Showing Customers how to wire either a NPN or PNP signal for a trigger. kA23800000008AWCAY_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 22 views
Here is the procedure to reset the Ethernet card: Note: Restoring the Ethernet card to its factory default settings will clear all current settings except the IP address settings and the administrator password. 1. Power off the scanner. 2. Separate the MS-890 from the wiring box using the four screws in the corners. 3. Locate the reset switch between P3 and CR1 on the Ethernet card. 3. Power on the scanner while holding the reset switch down. (Hold it down for about 20 seconds.)
Last reply by Omron Forums Support,