Jump to content
OMRON Forums

Updating the QX Hawk in Safe Mode


Recommended Posts

How to update the QX-hawk firmware when the unit does not respond to the normal auto connect. 1. Start the QX-Hawk in Safe mode. To do this , power the unit while keeping the Default pin (3) connected to the ground pin (7). In the standard QX cables, these are the green and blue wires. Keep the connection until the red cross comes on or for about 15 seconds. 2. Start ESP and force connect with communication settings 115,N,8,1. 3. Go to the ESP terminal. 4. Type and see if there is an answer. The unit should respond with the firmware versions and the text SAFE MODE. 5. Try to update the APP code which has been working before. The update can take more than 10 minutes. After the update, re-power the QX-Hawk. * If the update has succeeded, try to connect via Ethernet and update to the new Kernel, App code and the DSP code. In this order. * If the update has not succeeded, Force connect via RS-232 and update to the new Kernel, App code and the DSP code.

Link to comment
Share on other sites

  • Replies 0
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

Join the conversation

You can post now and register later. If you have an account, sign in now to post with your account.

Guest
Reply to this topic...

×   Pasted as rich text.   Paste as plain text instead

  Only 75 emoji are allowed.

×   Your link has been automatically embedded.   Display as a link instead

×   Your previous content has been restored.   Clear editor

×   You cannot paste images directly. Upload or insert images from URL.


×
×
  • Create New...