Code Reading
210 topics in this forum
-
- 0 replies
- 275 views
This guide will help you regain access to your camera if you have forgotten your camera login password. This will be achieve by deleting the camera's Weblink user settings configuration file. In order to delete this file we will need to connect to the camera via the ftp protocol. Instructions: 1. Open the windows command prompt program. 2. Type in the following command: a. ftp [CAMERA_IP _ADDRESS] b. Example i. ftp 192.168.188.2 3. Type in "target" for the User. Then click Enter. 4. Type in "password" for the Password. Then click Enter. 5. If the ftp login was successful, you should get a …
Last reply by Omron Forums Support, -
- 0 replies
- 226 views
To correct the "Runtime Display Not Available" message in FrontRunner, do the following: 1. Shut down the Visionscape FrontRunner software. 2. Close the Visionscape Backplane. 3. Open the Windows Registry Editor. 4. Delete the following key: HKEY_CURRENT_USER\SOFTWARE\Microscan\Visionscape\FrontRunner The next time the Visionscape FrontRunner software is started that registry key will be created and correct this problem.
Last reply by Omron Forums Support, -
The OMRON V410-H is capable of limited OCR (Optical Character Recognition) functionality. The reader can read 6 to 60 point OCR typeface and supports font types OCR-A, OCR-B, MICR-E13B, and US Currency Serial Number. As part of their widespread Microsoft Office suite, there are two built-in “OCR” fonts: “OCR-A Extended“ and “OCR-B-Seagull” Customers utilizing Word or other Microsoft products to create documents intended to utilize this V410-H functionality should be aware that these fonts are NOT supported by the V410-H OCR function. Despite the similar names, these Microsoft fonts are not actual analogues of true OCR-A or OCR-B and will not be detected by the scann…
Last reply by Omron Forums Support, -
- 0 replies
- 223 views
Last reply by Omron Forums Support, -
- 0 replies
- 195 views
Purpose: To return an OMRON Microscan barcode scanner to a known-good default state to re-establish communications. Explanation: In certain instances, communication with a barcode scanner may become impossible, often due to an unintentional change of settings to an unknown state. This may make certain default procedures unavailable. This procedure will allow you to default the reader, including communication settings, back to a known default state to allow the re-establishment of communications. Supported Products: All current AutoID products supported by ESP Procedure: 1. Open ESP. 2. Choose your product model from the “Model” window: 3. Answer “…
Last reply by Omron Forums Support, -
Purpose: This note will show how to verify the version of flash memory hardware used on any MicroHAWK or V/F4xx-family barcode scanner or smart vision camera. This is important information prior to attempting to update firmware past version 1.3 (for MicroHAWK ID or V4xx) or AutoVISION 5.0 (for MicroHAWK MV or F4xx) since doing so on an incompatible unit can result in loss of communication with the unit. Recovering units at that point generally requires specialized cabling and assistance from Technical Support. Steps Step 1 Connect to the device and open a telnet connection (all screenshots will show the use of Windows Telnet Client). Default IP address …
Last reply by Omron Forums Support, -
- 0 replies
- 342 views
1. Normal screen view after selecting camera 2. Use CTRL+SHIFT+ALT and select camera 3. New screen view
Last reply by Omron Forums Support, -
- 0 replies
- 211 views
Introduction Purpose: How to wire a momentary switch to unlatch an output. Explanation: The MS-Connect 210 does not allow the external membrane switches to be programmed for other uses. In order to unlatch an output, you will need to wire a separate momentary switch to “Input 1” on the inside terminal(s) of the MS-Connect 210. Supported Products: • All readers that allow Output X = Latch mode 1 (unlatch on Input # 1 pin) where X is the number of the Output in the I/O section of the reader settings. Typically called Output 1, 2, or 3. Here is a quick sketch showing the wiring of a switch to the terminals in the MS-Connect 210 The connections are as follows: …
Last reply by Omron Forums Support, -
- 0 replies
- 240 views
Introduction: Purpose: This document will describe the procedure to install additional feature licenses purchased for the MicroHAWK V3xx, V4xx, and ID-20 barcode readers. Explanation: The MicroHAWK family of barcode readers has the unique ability to use add-on licenses to enable additional features purchased at a later date (dependent on existing installed features). This is done through the installation of small license files. This procedure will be outlined here. Supported Devices: • MicroHAWK V320 • MicroHAWK v330 • MicroHAWK v420 • MicroHAWK v430 • MicroHAWK ID-20 What you will need: • MicroHA…
Last reply by Omron Forums Support,