Code Reading
202 topics in this forum
-
This is a bug in the firmware that was fixed in 35-338301-14. Download and install current firmware to resolve this error.
Last reply by Omron Forums Support, -
- 0 replies
- 198 views
The embedded Etherent interface of the QX products can only be configured as a server. No, they can not be configured as a client.
Last reply by Omron Forums Support, -
- 0 replies
- 220 views
This applies to the MS-Q, HE-40T, and HE-45T. Using the Shared Access mode in the Bluetooth section of the User's Manual will allow you to connect up to three handhelds into a single modem for real-time operation. You must use the Microscan Bluetooth modem (98-000076-xx) in order for this to work properly.
Last reply by Omron Forums Support, -
- 0 replies
- 444 views
Google Chrome (Recommended)Internet Explorer version 11 and aboveFirefoxOperaSafari (Mac Only)Microsoft Edge Browser Feature Requirements for WebLink WebLink requires certain features to be supported by the hosting browser. Support for these features are checked before WebLink loads, and if not available, an error dialog is shown. The following features are required by WebLink and are checked at start up: Web SocketsHTML 5 CanvasHTML 5 Audio OS Requirements for WebLink Windows XP (Must use non-IE browser)Windows 7Windows 10Note: Use of an Embedded OS (Windows CE) and / or an underpowered machine (limited RAM, disk space) is not recommended. Firmware …
Last reply by Omron Forums Support, -
- 0 replies
- 224 views
IMPORTANT NOTE ABOUT THE STITCHING FEATURE The entire process of stitching a label requires the user to correctly align the images being stitched. Failure to correctly align the labels results in the barcode being graded poorly. When in doubt, perform the stitching process again. Note that the stitching feature does not work for all barcodes. 1. Activate the Stitching feature by pressing the [Ctrl + S] keyboard buttons at the same time; the screen changes as shown in the screenshot below. 2. Adjust the image so the left edge of the linear barcode is visible and leave enough space for the left quiet zone (see screenshot on next page). 3. Line up the top of the barcode to…
Last reply by Omron Forums Support, -
- 0 replies
- 242 views
There are 3 different ways to get keyboard output from a barcode reader; Use a software wedge. A software wedge is a program that runs in the background on the host that converts almost any communication port data into keyboard strokes. TWedge and WinWedge are examples of 3rd party programs that convert barcode data being received via RS232 or TCP/IP into keyboard strokes.Use a hardware wedge. A hardware wedge is a cable or adapter that physically converts the RS232 or TCP/IP data into keyboard strokes. Microscan, Intelleto and MicroRidge are manufacturers of hardware wedges. Please remember if using an RS232 converter to match the baud rate of the wedge with the host po…
Last reply by Omron Forums Support, -
- 0 replies
- 289 views
Unit need to send back for repair. Below is the selftest resutl SELF TEST START, REINITIALIZING........ OK INTERNAL RAM TEST...................... OK 35-338200-13 .............CHECKSUM = 375B 35-338201-20 .............CHECKSUM = ABE3 EXTERNAL RAM TEST TESTING A0 TO A7 ...................... OK TESTING A8 TO A17...................... OK BYTE PATTERN TEST...................... OK WORD PATTERN TEST...................... OK NOVRAM TEST............................ OK CPU VIDEO INPUT TEST .................. OK VIDEO INPUT Default to White TEST ..... FAILED TESTING LASER ON MOTOR OFF CARRIAGE RETURN TO SKIP DELAY LASER CURRENT IS = 04.................. OK STARTING SCANNER INIT M…
Last reply by Omron Forums Support, -
- 0 replies
- 317 views
This document outlines the criteria for sending commands to the readers and describes the simple ASCII command structure. kA23800000008JLCAY_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 231 views
The ESP software does not allow the choice for updating Firmware in the MS-2 USB. The attached application note will show you how to perform the upgrade kA23800000008KbCAI_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 246 views
In this application example the Microscan Hand held reader (any RS-232 version) is wired to the Aux port of a Fixed mount RS-232 scanner With Matchcode capabilities. (Example MS-3) When the Hand held reads the symbol it will transmit and load into the Fixed mount as a master Symbol. kA23800000008DxCAI_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 230 views
This application example outlines how to connect and program two MS-3 barcode readers for Cross Match operation. kA23800000008AXCAY_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 219 views
Attached is a white paper describing how to configure any combination of QX device to do the “Cross Match” application. In this type of application One scanner will Teach the other what to look for. Then the second scanner will either Match or Mismatch to that code. Note* The “Teach” scanner could also be an Ethernet version as you only need Port A on the scanner. kA2380000000870CAA_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 227 views
The following configuration will allow two separate labels to be compared to each other. Between the two scanners, three outputs can be taken to define the results of the complete cycle: Noread, Match and Mismatch. If desired, you can also collect RS-232 information in the case of a match or a mismatch. kA23800000008AFCAY_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 239 views
If the hole pattern of 98-000016-01 does not fit the screw pattern of QX Hawk and the holes are round, it is an old revision. New parts of 98-000016-01 have slotted holes that will fit all QX products, including the QX Hawk. See attached image for reference.
Last reply by Omron Forums Support, -
- 0 replies
- 231 views
1. Open ESP and connect to the QX-Hawk reader 2. Select the Parameters Icon 3. Select the Symbol Quality sub tab 4. Under Datamatrix/Grading, enable Symbol Angle 5. Verify output
Last reply by Omron Forums Support, -
- 0 replies
- 203 views
Introduction: Purpose: This document will describe the procedure to install additional feature licenses purchased for the MicroHAWK V3xx, V4xx, and ID-20 barcode readers. Explanation: The MicroHAWK family of barcode readers has the unique ability to use add-on licenses to enable additional features purchased at a later date (dependent on existing installed features). This is done through the installation of small license files. This procedure will be outlined here. Supported Devices: MicroHAWK V320 MicroHAWK v330 MicroHAWK v420 MicroHAWK v430 MicroHAWK ID-20 What you will need: MicroHAWK Barcode Reader FTP client software (FileZilla Cli…
Last reply by Omron Forums Support, -
- 0 replies
- 230 views
The purpose of this tech note is to re-enable Bluetooth Radio after a user has scanned the code below. Until this gets fixed, the only way to re-enable is detailed below. Download the following zip file. https://adept.box.com/s/ci512petttk0cu3z8bbtmgtbe7v9qp87 Extract to a location on your hard drive Open a command prompt and navigate to that folder Execute the setattrib.bat file passing the serial number of the cradle to the bat file: As shown above, you should see at the end of the garbled response “Success”. Re-scan the restore defaults barcode on the scanner Then pair it to the cradle again by scanning the pairing symbol on…
Last reply by Omron Forums Support, -
- 0 replies
- 153 views
Boot firmware will have to be updated using the RS232 connection instead of the Ethernet connection. There is also an additional step required for the Boot firmware update and will require a flying leads cable. This guide will show the steps using a QX-1 configuration. 1. Power down the QX-830. 2. Connect the QX-830 to port '2' of the QX-1 . 3. Connect the Flying Lead cable to port '1' of the QX-1 (make sure the wires are not being shorted!). 4. Connect the Power Supply to port '3' of the QX-1. 5. Locate pin 3 (Default, Green) and pin 7 (OV, Blue) and connect them together. 6. Power up the QX-830, the 20%, 40% and 60% LEDs will start blinking to indicate…
Last reply by Omron Forums Support, -
- 0 replies
- 339 views
This guide will help you regain access to your camera if you have forgotten your camera login password. This will be achieve by deleting the camera's Weblink user settings configuration file. In order to delete this file we will need to connect to the camera via the ftp protocol. Instructions: 1. Open the windows command prompt program. 2. Type in the following command: a. ftp [CAMERA_IP _ADDRESS] b. Example i. ftp 192.168.188.2 3. Type in "target" for the User. Then click Enter. 4. Type in "password" for the Password. Then click Enter. 5. If the ftp login was successful, you should get a …
Last reply by Omron Forums Support, -
- 0 replies
- 261 views
To correct the "Runtime Display Not Available" message in FrontRunner, do the following: 1. Shut down the Visionscape FrontRunner software. 2. Close the Visionscape Backplane. 3. Open the Windows Registry Editor. 4. Delete the following key: HKEY_CURRENT_USER\SOFTWARE\Microscan\Visionscape\FrontRunner The next time the Visionscape FrontRunner software is started that registry key will be created and correct this problem.
Last reply by Omron Forums Support, -
The OMRON V410-H is capable of limited OCR (Optical Character Recognition) functionality. The reader can read 6 to 60 point OCR typeface and supports font types OCR-A, OCR-B, MICR-E13B, and US Currency Serial Number. As part of their widespread Microsoft Office suite, there are two built-in “OCR” fonts: “OCR-A Extended“ and “OCR-B-Seagull” Customers utilizing Word or other Microsoft products to create documents intended to utilize this V410-H functionality should be aware that these fonts are NOT supported by the V410-H OCR function. Despite the similar names, these Microsoft fonts are not actual analogues of true OCR-A or OCR-B and will not be detected by the scann…
Last reply by Omron Forums Support, -
- 0 replies
- 244 views
Last reply by Omron Forums Support, -
- 0 replies
- 229 views
Purpose: To return an OMRON Microscan barcode scanner to a known-good default state to re-establish communications. Explanation: In certain instances, communication with a barcode scanner may become impossible, often due to an unintentional change of settings to an unknown state. This may make certain default procedures unavailable. This procedure will allow you to default the reader, including communication settings, back to a known default state to allow the re-establishment of communications. Supported Products: All current AutoID products supported by ESP Procedure: 1. Open ESP. 2. Choose your product model from the “Model” window: 3. Answer “…
Last reply by Omron Forums Support, -
Purpose: This note will show how to verify the version of flash memory hardware used on any MicroHAWK or V/F4xx-family barcode scanner or smart vision camera. This is important information prior to attempting to update firmware past version 1.3 (for MicroHAWK ID or V4xx) or AutoVISION 5.0 (for MicroHAWK MV or F4xx) since doing so on an incompatible unit can result in loss of communication with the unit. Recovering units at that point generally requires specialized cabling and assistance from Technical Support. Steps Step 1 Connect to the device and open a telnet connection (all screenshots will show the use of Windows Telnet Client). Default IP address …
Last reply by Omron Forums Support, -
- 0 replies
- 409 views
1. Normal screen view after selecting camera 2. Use CTRL+SHIFT+ALT and select camera 3. New screen view
Last reply by Omron Forums Support,