Omron Forums Support Posted March 8, 2022 Share Posted March 8, 2022 Introduction:Purpose: This document will describe the procedure to install additional feature licenses purchased for the MicroHAWK V3xx, V4xx, and ID-20 barcode readers. Explanation: The MicroHAWK family of barcode readers has the unique ability to use add-on licenses to enable additional features purchased at a later date (dependent on existing installed features). This is done through the installation of small license files. This procedure will be outlined here.Supported Devices: MicroHAWK V320 MicroHAWK v330 MicroHAWK v420 MicroHAWK v430 MicroHAWK ID-20 What you will need: MicroHAWK Barcode Reader FTP client software (FileZilla Client used in this example) MicroHAWK feature license file (.lic file) Instructions: 1. Connect the MicroHAWK to the Ethernet network or the PC. 2. Open FileZilla FTP Client and following info into the corresponding fields at the top: Host: Your MicroHAWK’s IP address (default is 192.168.188.2). Username: target Password: password 3. In the upper-right pane navigate to /sd0:0/Config/Licensing. 4. Copy your .lic feature license file to the Licensing folder. 5. Close FileZilla Client and reboot or power cycle your MicroHAWK. 6. Your newly-licensed feature should now be active on your MicroHAWK Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.