Omron Forums Support Posted March 7, 2022 Share Posted March 7, 2022 Purpose: This note will show how to verify the version of flash memory hardware used on any MicroHAWK or V/F4xx-family barcode scanner or smart vision camera. This is important information prior to attempting to update firmware past version 1.3 (for MicroHAWK ID or V4xx) or AutoVISION 5.0 (for MicroHAWK MV or F4xx) since doing so on an incompatible unit can result in loss of communication with the unit. Recovering units at that point generally requires specialized cabling and assistance from Technical Support.Steps Step 1 Connect to the device and open a telnet connection (all screenshots will show the use of Windows Telnet Client). Default IP address is 192.168.188.2 if still using defaults. Step 2 Log in to the device shell using the following credentials: Username: target Password: password Step 3 Type the command SeeFlashID() (in yellow below). The information we are seeking is highlighted in red below. If the response says SST25 then the unit has the older flash memory which is compatible with all versions of firmware and no further action is necessary. If the response says SST26 then the unit has the new flash memory hardware. This new hardware MUST be used with firmware version 1.3 (for MicroHAWK ID or V4xx) or AutoVISION 5.0 (for MicroHAWK MV or F4xx) or NEWER to function. Use of any firmware versions older than this on a unit with the new flash memory hardware will result in a soft “bricking” of the unit which can only be recovered through the use of RS232 cabling and likely will require assistance from Technical Support. Note: Only units made after approximately May 2018 have the new SST26 flash memory. If in doubt, run this check. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.