Omron Forums Support Posted March 7, 2022 Share Posted March 7, 2022 This guide will help you regain access to your camera if you have forgotten your camera login password. This will be achieve by deleting the camera's Weblink user settings configuration file. In order to delete this file we will need to connect to the camera via the ftp protocol.Instructions: 1. Open the windows command prompt program. 2. Type in the following command: a. ftp [CAMERA_IP _ADDRESS] b. Example i. ftp 192.168.188.2 3. Type in "target" for the User. Then click Enter. 4. Type in "password" for the Password. Then click Enter. 5. If the ftp login was successful, you should get a "Login OK" message. 6. Enter the following command to delete the settings.json file. a. delete /sd0:0/http/user/settings.json 7. If the delete command was successful, you should get a "File Deleted" message. The camera's login feature should now be defaulted and turned off. The windows command prompt program can now be closed. 8. The camera's Weblink interface can now be opened to double check the login requirement is no longer needed. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.