Omron Forums Support Posted March 8, 2022 Share Posted March 8, 2022 Purpose: Completely uninstall and re-install the LVS-95XX software. Explanation: In certain situations, it may be necessary to thoroughly and completely uninstall the LVS-95XX software and any residual settings in order to resolve a given error or issue. This facilitates the reinstallation of the software onto the PC from a completely fresh state, as if it was the first time the software had ever been installed. 1. Begin by uninstalling the LVS-95XX software itself. You can do this by going to Control Panel > Programs and Features, as shown below. Then simply follow the prompts to uninstall. 2. Next, uninstall the accompanying drivers, as shown in the screenshot below. The process will mirror Step 1. 3. Next, you will need to delete the existing registry key. Start the Registry Editor by typing “regedit.exe” into the Windows search box, as shown below. Next, delete the registry key highlighted in the second screenshot at one of the following paths: HKEY_LOCAL_MACHINE > SOFTWARE > Wow6432Node > Microscan > LVS-95XX > Database or HKEY_LOCAL_MACHINE > SOFTWARE > Label Vision Systems > Database. 4. All Integra 95XX components should now be uninstalled and the PC should be ready for a new installation. If you have the original CD or USB installation media that came with your verifier, you may now insert it and reinstall the software according to the guidelines specified in the LVS-95XX Series Software Installation Guide. If you have been provided a download link for the software, extract the files, then continue to follow the installation guidelines mentioned previously.5. Once the software has been successfully reinstalled, copy your .mdb file for you verifier to the new folder location. On your original installation media, in the “LVS-95XX” folder, is a file named “i95xx_yyyyy.mdb”, with “xx” being the rest of the model number of your verifier and “yyyyy” being its serial number. This file should be copied and placed in the appropriate folder listed below and renamed appropriately:If you installed 3.0.9qq or earlier: Move to “C:\Users\Public\I9500”; rename to “I9500.mdb”.If you installed 4.0.0h or later: Move to “C:\Users\Public\LVS-95XX”; rename to “LVS-95XX.mdb”.6. Once installation is complete, plug in the verifier and attempt to login to the software with the below credentials to confirm that the install was successful:Operator ID: adminPassword: admin Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.